How embedded cameras enable city safety using security cameras

As urban populations continue to grow, cities face numerous safety challenges. Citizens’ safety and property protection are constantly at risk, from minor thefts to more serious crimes. While traditional methods like policing and community watch programs have some success, they struggle to keep up with the changing landscape of urban safety concerns.

Introducing embedded cameras – these cameras are seamlessly integrated into the city’s infrastructure and provide continuous real-time monitoring of public spaces. Not only do they act as a deterrent for potential criminals, but their footage also proves valuable in crime investigation and prosecution efforts. With human surveillance limitations, embedded cameras offer efficient monitoring on a larger scale.

VCI-AR0521-SL – For smart city applications

Challenges of ensuring safety in a large city

Ensuring safety in a large city presents several challenges.

  • One major challenge is the diverse range of crimes that cities must address, from small-scale theft to larger organized criminal activities. This requires adaptable and versatile safety strategies to effectively combat these various types of crime.
  • Another challenge is allocating limited resources, such as personnel and funding, to the most critical areas where they will have the greatest impact on keeping the city safe. Finding a balance between these competing demands is an ongoing struggle for large cities.
  • Technological integration is a complex process of implementing various technologies for monitoring and response. This is crucial for effective law enforcement and crime prevention.
  • Equally important is gaining and maintaining the community’s trust, which fosters cooperation and collaboration between law enforcement agencies and citizens.
  • Rapid urbanization can often outpace safety measures and infrastructure, leading to potential resident risks. In navigating legal frameworks and ethical concerns, especially about surveillance and enforcement methods, it is crucial to consider the consequences of rapid growth and changing urban landscapes.
  • Coordination and swift action are key in effectively responding to emergencies such as crimes or natural disasters, which can be quite challenging.

How embedded cameras can help with security in a city

Cameras play a crucial role in enhancing security in cities. They deter potential criminals by signaling that they are under surveillance, significantly reducing the likelihood of criminal activities.

In addition, video footage captured by these cameras can help identify suspects, confirm alibis, and provide court-admissible evidence. Real-time monitoring also allows for immediate detection of crimes or suspicious activities, enabling law enforcement to respond quickly and effectively.

Traffic regulation is made easier with cameras, which monitor traffic flow and detect violations. They also play a crucial role in post-accident investigations, creating safer roads for everyone. In addition, surveillance systems are useful for crowd monitoring during large events, as they can spot potential disturbances and manage the flow of people to ensure public safety.

Also read: How Embedded Cameras are Powering New-age Smart Traffic Systems

Smart Surveillance

In emergencies, cameras can provide real-time assessment of affected areas, aiding in efficient rescue and relief operations. Their advanced features, like anti-fogging and multi-camera setups, also ensure clear and comprehensive coverage for surveillance purposes.

Additionally, integration with AI allows for automatic recognition of suspicious behaviors, face recognition, and tracking movements in crowded spaces. This data analytics capability can greatly enhance security measures in high-risk environments.

Benefits of using smart surveillance cameras

  • Smart cameras offer enhanced monitoring and security, providing continuous surveillance for a more secure environment. Compared to intermittent human monitoring, these cameras are more efficient and less prone to errors. With their advanced technology, you can have peace of mind knowing your space is constantly monitored.
  • Automated alert systems and real-time response capabilities utilize advanced AI technology to detect and notify authorities of unusual activities. This significantly speeds up incident response time, reducing reliance on human observation and potential delays.
  • Surveillance footage is crucial in crime investigation and prosecution, providing clear evidence for successful prosecution. Additionally, advanced features like anti-fogging ensure clear vision in all weather conditions, making it easier to adapt to changing environmental conditions. Embedded cameras make this impossible, making surveillance solutions an essential tool for law enforcement agencies.
  • Multi-camera systems offer comprehensive coverage for monitoring large areas, while single-camera setups may leave blind spots. This is crucial for managing traffic and large public gatherings, as smart cameras can identify potential risks and help streamline crowd control measures. With multi-camera systems, businesses can ensure efficient coverage and management of their premises or events.
  • In times of crisis, real-time situational awareness is crucial for a coordinated response. Smart cameras and other advanced technologies provide this essential information, making emergency response more informed and effective.
  • With the ability to quickly identify individuals, smart cameras play a vital role in locating missing persons or suspects. Manual identification would be far more time-consuming and less accurate without this technology.
  • Integrating these cameras with other security systems allows for comprehensive coverage, providing greater protection. Additionally, the AI algorithms used in these cameras can analyze behavior patterns and predict potential criminal activities, enhancing the overall effectiveness of the surveillance system.
  • Smart surveillance can lead to the efficient use of law enforcement resources. This technology can also increase public confidence in safety measures by utilizing visible cameras and archived footage for historical data analysis. This allows for studying long-term trends and planning future safety measures, enhancing community safety perception.

Key features of smart surveillance cameras

Embedded cameras used in smart surveillance systems need to come with certain features to ensure smooth operation. Let’s look at all such necessary features here.

  • Night vision (NIR sensitivity): This feature allows cameras to take clear images in dim or dark environments, which is essential for ongoing surveillance, particularly in places with minimal lighting. For this, a camera with superior NIR (Near InfraRed) sensitivity has to be used. This makes it possible to capture images even in 0 lux conditions.
    TechNexion’s camera solutions for surveillance and security come with high QE (Quantum Efficiency) values in the NIR spectrum. This ensures that our cameras can operate effectively even during the night.
  • PTZ (Pan, Tilt, Zoom): Provides surveillance versatility by enabling operators to remotely control the orientation and zoom of the camera for comprehensive viewpoints of a select region. This also ensures that the complete area under surveillance can be covered.
  • High resolution: Ensures that recorded images are clear and detailed, which is necessary for distinguishing faces, license plates, and other important information in surveillance footage. In most cases, a 5MP camera would suffice. However, modern security camera systems have become more demanding and might require higher quality images. In such cases, a camera with a resolution of 8MP can be chosen.
  •  Multi-camera synchronization: This function ensures multiple cameras operate in unison to provide comprehensive and seamless coverage, making it useful for covering large areas. Depending on the field of view to be covered, one camera system might have to use 2 to 3 cameras. In most cases, the practice is to use a single camera. However, if broader coverage is required, multiple camera modules can be used.
  • Wide field of view: A wide field of view is extremely important, especially if you are using a single camera system. A camera with a minimum field of view of 70 degrees is recommended. At the same time, the choice of the lens (which is what determines the field of view) also depends on several other factors such as the sensor used, scene of interest, working distance, etc. So, make sure to factor in all of them before you choose a lens with a particular field of view.
UVCI-AR0522-SL Medium FOV Right

USB3 Type-C PCB Board Camera with onsemi AR0522 5MP Rolling Shutter with Onboard ISP and S-mount Lens

In stock Out of stock On backorder

UVCI-AR0522-SL

  • onsemi AR0522 5MP Rolling Shutter Sensor
  • Near Infra-Red Enhancement for Outdoor Applications
  • Designed for Low Light Applications
  • S-Mount for Interchangeable Lenses
  • UVC USB Type-C 5 Gbps Connector
  • Plug & Play with Windows & Linux OS
  • VizionViewer™ configuration utility
  • VizionSDK for custom development
  • High Dynamic Range: High dynamic range or HDR adjusts the lighting in the video stream, guaranteeing clear images even in direct sunshine or dark locations. It is ideal for situations with different lighting conditions. If the system must operate in a location that is under bright light quite often, a camera with a dynamic range of 120 dB or above is recommended.
  • IP-rated enclosure: Offers reliable performance and long-term protection for cameras against adverse weather conditions, dust, and high temperatures. For instance, TechNexion’s cameras come with an IP68-rated enclosure that offers excellent protection even in the harshest external and industrial conditions.
  • Anti-fogging: This feature keeps the lens from fogging, essential for keeping clear vision in humid or fluctuating temperature environments, always ensuring the camera’s efficacy.

TechNexion – embedded cameras for security systems

TechNexion is a leading provider of embedded cameras for security systems, offering advanced surveillance capabilities. Our cameras improve security by providing a wider field of view, more accurate object tracking, and reduced lens distortion. They can be used in smart surveillance systems installed in traffic junctions, parks, sports arenas, busy streets, etc.

With key features such as NIR sensitivity, high resolution, low light performance, and high dynamic range, they are an excellent fit for any kind of surveillance application. Learn more about our embedded cameras here.

We also have a state-of-the-art manufacturing facility that comes with the PoP (Package on Package) technology. We also conduct rigorous quality tests to ensure that our cameras have a long life even in the toughest industrial and environmental conditions. Learn more about our manufacturing capabilities here.

SHARE YOUR CART